Edmund Optics® has introduced a line of Omega Optical DUV Transmission Gratings designed for peak performance in the deep ultraviolet (DUV) spectrum—available off-the-shelf. These award-winning gratings were recognized with a 2025 SPIE Prism Award for their breakthrough performance in the deep ultraviolet range—underscoring their innovation and impact in optical engineering. These gratings are uniquely optimized for wavelengths as short as 190 nm, a range where conventional optical components often fail due to material and efficiency challenges.
Offering excellent first-order diffraction efficiency below 200 nm, these gratings enable more usable light in critical applications such as high-resolution spectroscopy, advanced lithography, and precision biomedical instrumentation. Customers benefit from better diffraction efficiencies, improved system throughput, and seamless availability—without the delays of custom sourcing.
Unlike other solutions that require special order, Edmund Optics provides these cutting-edge DUV gratings off the shelf on their e-commerce website for immediate purchase. Customers now have a streamlined path to high-performance DUV integration, backed by Edmund Optics’ extensive inventory and expert support.
About Edmund Optics®:
With over 80 years of experience, Edmund Optics® is a trusted provider of high-quality optical components and solutions, serving industries like Life Sciences, Biomedical, Industrial Inspection, Semiconductor, and R&D. The company employs 1,300+ people across 19 global locations and continues to grow.
As a leading optics and photonics company, Edmund Optics provides two specialized solutions: a robust Marketplace with 34,000+ off-the-shelf products and Advanced Manufacturing, which focuses on custom and volume production of precision optical and imaging components.
Edmund Optics’ Marketplace is a one-stop shop for over 34,000 in-stock products from in-house manufacturing and 40+ top-tier brands, covering the entire beam path with fast, easy purchasing. For tailored solutions, Advanced Manufacturing offers custom design, first-article production, and scalable manufacturing — supported by four global design centres and nine specialized factories producing over 2 million components and 175,000+ assemblies annually.
Learn more at www.edmundoptics.com
Contact:
Agnes Huebscher, Senior Director, Global Corporate Marketing and Communications
[email protected]
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023 | Edmund Optics, Ltd Unit 1, Opus Avenue, Nether Poppleton, York, YO26 6BL, UK
California Consumer Privacy Acts (CCPA): Do Not Sell or Share My Personal Information
California Transparency in Supply Chains Act
This content may include material that has been generated or modified using artificial intelligence (AI).
The FUTURE Depends On Optics®