Edmund Optics uses cookies to optimise and enhance the features and content on our website. By continuing to use this website, you consent to our use of cookies.

  • My Account
  •   
Resource Page / Application Notes / Imaging / Telecentric Design Topics
Telecentric Design Topics
Edmund Optics Inc.

Telecentric Design Topics

This is Section 5.4 of the Imaging Resource Guide

In previous sections, the lenses discussed have been divided into two different categories: Telecentric Lenses and non-telecentric lenses. However, there are two types of telecentricity: object space and image space telecentricity (which refer to the entrance pupil and exit pupil locations, respectively). The pupils of an optical system are images of the aperture stop; typically, machine vision lenses have embedded aperture stops, with individual lens components surrounding it on either side. The entrance pupil is the image of the aperture stop into image space, and the exit pupil is the image of the aperture stop into object space. See Figure 1 for illustrations of entrance and exit pupils for a non-telecentric lens.

A Machine Vision Lens with Entrance and Exit Pupils located within the Lens
Figure 1: A Machine Vision Lens with Entrance and Exit Pupils located within the Lens, which is typical of most Fixed Focal Length Lenses

Object Space Telecentricity

When a machine vision lens is described as simply being telecentric, it is most likely object space telecentric. These have all of the properties and advantages described in the previous sections. A lens is said to be object space telecentric when the entrance pupil is located at infinity in image space (everything behind the objective), as shown in Figure 2.

A Lens which is Object Space Telecentric, with the Entrance Pupil projected to Image-Side Infinity
Figure 2: A Lens which is Object Space Telecentric, with the Entrance Pupil projected to Image-Side Infinity

In an optical design, object space telecentricity is accomplished by placing the aperture stop of the system at the focal point of the front group. The entrance pupil at infinity explains why the field of view is constant and non-angular. Since the chief ray, which defines the field of view of a system, crosses the optical axis at the aperture stop and also crosses at the entrance pupil, the ray will be parallel to the optical axis when the pupil is at infinity, and the angular field of view is zero (Figure 3). By contrast, any entrance pupil located a finite distance away from the lens will result in a non-parallel chief ray, as shown traced in Figure 4 for a non-telecentric lens.

An Object Space Telecentric Lens, where the Chief Rays are all Parallel to the Optical Axis in Object Space
Figure 3: An Object Space Telecentric Lens, where the Chief Rays are all Parallel to the Optical Axis in Object Space. Note that the field of view does not change regardless of where the object plane is positioned, as the chief rays defining the field of view are all parallel to the optical axis
The Entrance Pupil’s location is where the Object Space Chief Ray crosses the Optical Axis
Figure 4: The Entrance Pupil’s location is where the Object Space Chief Ray crosses the Optical Axis, as shown with a Non-Telecentric Lens

Lenses that are only object space telecentric have the ability to be focusable since the back half of the lens can be designed with moving elements, which is advantageous for systems that need the variability of working distance. They can also be designed to be variable magnification lenses, as the rear elements can be used to control magnification, or the sensor plane can be moved for small magnification shifts. The magnification in the field of view, however, will still remain constant once the magnification is set, and will retain the high measurements accuracy that is expected of a Telecentric Lens.

Object space-only Telecentric Lenses are more easily capable of hitting larger image sensor formats, even in more compact form factors, as the rays in image space are allowed to diverge; the back of the lens therefore does not need to exceed the sensor dimensions.

Image Space Telecentricity

As object space telecentricity is defined by the position in object space of the entrance pupil, image space telecentricity can be defined by the exit pupil being located at infinity in object space. This is shown in Figure 5.

A Lens which is Image Space Telecentric, with the Exit Pupil projected to Image Space Infinity
Figure 5: A Lens which is Image Space Telecentric, with the Exit Pupil projected to Image Space Infinity

Much in the same way that the magnification of an object will not change if a lens is object space telecentric, when a lens is image space telecentric the magnification will not change with respect to the placement of the sensor plane, as shown in Figure 6. This means that sensor placement tolerance for cameras is not as important with image space telecentric lenses, as small shifts toward or away from optimal position will not cause differences in magnification between two systems with identical lenses.

An Image Space Telecentric Lens, where the Chief Rays are all Parallel to the Optical Axis in Image Space
Figure 6: An Image Space Telecentric Lens, where the Chief Rays are all Parallel to the Optical Axis in Image Space. Note that the image height does not change regardless of where the sensor plane is positioned, as the chief rays defining image height are all parallel to the optical axis

Additionally, image space Telecentric Lenses do not suffer from radiometric cos4θ roll-off (described in detail in Sensor Relative Illumination, Roll Off and Vignetting) since the rays land perpendicular to the sensor across its entire area. This is advantageous because it allows the image to have a more even relative illumination profile assuming selective vignetting has not been built into the lens design.

Image space telecentricity is not exclusive to Telecentric Lenses as it can be specified into conventional lenses such as Fixed Focal Length Lenses. Most Fixed Focal Length Lenses on the market are not designed to be image space telecentric, however, as they usually require additional elements (and thus cost) to achieve telecentricity, and they can grow quite large in diameter depending on the sensor size that is being used. If a non-telecentric lens is image space telecentric, it will typically be denoted.

Double Telecentricity

While object space telecentricity provides a substantial boost to gauging accuracy over conventional lenses, even greater accuracy can be achieved if a lens is both object and image space telecentric (doubly telecentric). The same principles of image and object space telecentricity hold true; in a doubly telecentric lens, both the entrance and exit pupils are projected to their respective infinities, as shown in Figure 7.

A Doubly Telecentric Lens, with the Entrance and Exit Pupils projected to Image and Object Space Infinity
Figure 7: A Doubly Telecentric Lens, with the Entrance and Exit Pupils projected to Image and Object Space Infinity, respectively

Doubly Telecentric Lenses are the most accurate type of Telecentric Lens, as the field of view is completely unaffected to change caused by shifts of the object position or the sensor position, nor do they suffer from any cos4θ roll-off.

Figure 8 shows a plot comparing three different lenses - a fixed focal length lens, an object space only telecentric lens, and a doubly telecentric lens - with the x-axis representing the change in working distance (in mm) from nominal and the y-axis representing the dimensional error as a percentage from the actual value.

Plot comparing three different Types of Lenses
Figure 8: Plot comparing three different Types of Lenses (Non-Telecentric, Object Space Telecentric, and Doubly Telecentric) and the Dimensional Error that is associated with each as the Working Distance is changed

As is shown in the plot, the doubly Telecentric Lens is the most accurate of the group, with less than 0.2% error throughout a 4mm shift in working distance. Doubly Telecentric Lenses should be used in applications requiring the highest accuracy and precision.

Was this content useful to you?

With over 800 Imaging Lenses and 40 pages of in depth Technical Content, make Edmund Optics Your Partner in Imaging Optics.

Perspective Errors are part of everyday human experience. Choose TECHSPEC® Telecentric Lenses to optically correct these errors in metrology or inspection applications. (PDF 1.30MB)

Free training videos with imaging and illumination tips and tricks.

Large format, compact, in-line, focus adjustment, or iris adjustment options available for your machine vision or inspection application.

Edmund Optics can not only help you learn how to specify the right imaging optics, but can also provide you with multiple resources and products to surpass your imaging needs.

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram

×