Edmund Optics uses cookies to optimise and enhance the features and content on our website. By continuing to use this website, you consent to our use of cookies.

  • My Account
  •   
Resources / Application Notes / Optics / High Laser Damage AR Coatings
High Laser Damage AR Coatings

High Laser Damage AR Coatings

Laser Damage Threshold (LDT), also known as Laser Induced Damage Threshold (LIDT), is one of the most important specifications to consider when integrating an optical component into a laser application. The type of damage induced to an optical component by a laser beam is dependent on its wavelength, pulse length, polarization, repetition rate, and spatial characteristics, among other factors. The failure mechanism of the optic is related to either the substrate or coating. The table below lists the most common variables that affect LIDT:

High Laser Damage AR Coatings
Variables that Affect LDT/LIDT
Laser Substrate Coating
Output Power Material Deposited Material
Pulse Duration Surface Quality Deposition Process
Pulse Repetition Rate Cleanliness Pre-Coating Preparation and Cleaning
Beam Profile Reactivity to the Environment Lot-to-Lot Control
Beam Diameter (1/e2) Material Absorption Coating Design and Optimization
Wavelength Material Homogeneity Protective Layers

Edmund Optics® specifies many of its AR Coated TECHSPEC® optical lenses with either a Laser Damage Threshold or a Typical Energy Density Limit.

Lenses designated with a Laser Damage Threshold have been designed, and guaranteed, to withstand a certain level of laser fluence. Extreme care is ensured throughout substrate preparation, cleaning processes, material choices, coating design and deposition processes, and packaging to ensure the lenses will not be damaged by the specified laser parameters. All processes have been meticulously documented and lenses manufactured with those processes have been rigorously tested by independent testing houses via the ISO-21254 procedures and methods.

Lenses designated with a Typical Energy Density Limit are coated with an anti-reflection (AR) coating that has been shown to withstand the specified laser parameters. The lens substrates are manufactured according to Edmund Optics’ world class manufacturing processes and standards, but have not been specifically designed to withstand high energy lasers.

Whether a lens has a guaranteed laser damage threshold or a typical energy density limit, the ultimate performance of the lens is highly dependent upon the environment in which it is used. To maximize the lifetime and performance of your lens, visit our website for application notes on proper handling, cleaning, and storage of laser optics.

Related Products

Was this content useful to you?

Edmund Optics is committed to ensuring product and procedural quality. Our products undergo a strict global quality program with rigorous and thorough testing.

Need to contact Edmund Optics? Use any of our fast and friendly services to meet your needs.

Since 1942, EO has been a leading supplier of optics and optical components. Learn more about our past, present, and future!

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram

×