Edmund Optics uses cookies to optimise and enhance the features and content on our website. By continuing to use this website, you consent to our use of cookies.

  • My Account
  •   
Resources / Glossary / J

Glossary: J

Jitter

An imaging phenomenon that limits the accuracy of measurement to at least two pixel separations because signals impinging on the sensor may fall on a pixel or on the space between pixels. Statistically speaking, the latter case may cause a response in the pixel to the immediate left or the immediate right of the space. Due to the standard scan frequency of 60Hz, such a static image will exhibit jitter between the two pixels in question over time. 

  See also Pixel

Spherical optics, aspheric lenses, prisms, imaging lenses, imaging and laser optics assemblies, and mechanics are just a few of our expertise.

Edmund Optics' engineers are experts in delivering the best solution possible. From stock products to custom designs, EO has the industry and technical knowledge to help meet your needs.

Over 15 regional offices in the Americas, Europe, and Asia to offer local support with world-class service.

Need to contact Edmund Optics? Use any of our fast and friendly services to meet your needs.

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram

×