Edmund Optics uses cookies to optimise and enhance the features and content on our website. By continuing to use this website, you consent to our use of cookies.

  • My Account
  •   
Resources / Glossary / E

Glossary: E

Eccentricity

The difference in alignment between the optical axis and the mechanical axis of a component, typically specified with a mirror.

Edge Thickness (ET)

A calculated value which depends on radii, diameter, and center thickness of a lens. It is thus used as a reference to indicate physical limitations for mounting considerations.

Effective Focal Length (EFL)

An optical measurement given as the distance from the rear principal plane of an optical system to its imaging plane, with an object located at infinity. Determines angular field of view of a lens.

Electronic Shutter

Controls the amount of time a camera collects light or charge during each frame, also known as the exposure time. Standard signal formats employ approximately 60 frames per second (fps), indicating a collecting charge of 1/60 seconds for each frame. As light levels increase the sensor overfills with charge, resulting in blooming or streaking. Electronic shuttering circuits prevent these effects by allowing the sensor to collect charge for a shorter period during each frame.

Electrostatic Discharge (ESD)

Built up charge through the action of static electricity that discharges into a person or device after contact. While ESD voltages frequently exceed 3,000 volts, the current associated with ESD is low making it safe, though at times unpleasant, for humans.

Ellipticity

The quality of asymmetrical intensity distribution in a laser beam, as opposed to a circular distribution.

Encoder

Electromechanical device that creates discrete electrical pulses directly related to the angular position of the input device (shaft). This allows for high resolution feedback data on position. 

Entrance Pupil

The image of the aperture stop through the lens elements preceding it into object space. 

  See also Marginal Ray , Exit Pupil , Chief Ray

Equilateral (Dispersing) Prism

A dispersion prism used to separate white light into its spectral components.  It has three equal 60° angles.

  See also Dispersion

Exit Pupil

The image of the aperture stop through the lens elements following it into image space.

Extinction Ratio

The relationship between the intensity of incident light to intensity of transmitted light passing through an optic.  It is used to categorize a polarizer or laser's ability to pass a given polarization state relative to another.

  See also Polarization

Spherical optics, aspheric lenses, prisms, imaging lenses, imaging and laser optics assemblies, and mechanics are just a few of our expertise.

Edmund Optics' engineers are experts in delivering the best solution possible. From stock products to custom designs, EO has the industry and technical knowledge to help meet your needs.

Over 15 regional offices in the Americas, Europe, and Asia to offer local support with world-class service.

Need to contact Edmund Optics? Use any of our fast and friendly services to meet your needs.

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram

×