Edmund Optics uses cookies to optimise and enhance the features and content on our website. By continuing to use this website, you consent to our use of cookies.

  • My Account
  •   
Resources / Glossary / Glossary

Glossary

IEC Laser Class

A laser class standard administered by the Commission Electrotechnique Internationale, which pubishes international standards for electronic components. It is an an alternative to the CDRH laser class standard used throughout North America.

  See also CDRH Laser Class

Image Capture Board (Frame Grabber)

A computer card that samples and digitizes analog video signals so that the information may be processed, stored, or operated on by the computer. Ideal for analog cameras because they have no computational software or digital cameras to maximize bandwith by transmitting data from large sensors at high frame rates. 

  See also Analog Signal , Digital Signal

Image Circle

The diameter of the maximum usable image produced by an imaging lens. 

Index of Refraction (n)

The ratio of the speed of light in a vacuum (c) to the speed of light in a refractive material (v). The index of refraction of a given medium varies with wavelength because the speed of light varies with wavelength. Common indices of refraction include n(the yellow helium line at 587.6nm), nf  (the blue hydrogen line at 486.1nm) and nc (the red hydrogen line at 656.3nm).

Infinite/Finite Conjugate

A conjugate distance relationship that combines two processes by focusing a source placed at infinity down to a spot. In terms of imaging, the object is placed at infinity (defined as the distance at which light rays can be considered collimated) in relation to the optical elements and imaged a finite distance onto a sensor or other image plane.

Infinite/Infinite Conjugate

A conjugate distance relationship that takes collimated light, changes the beam diameter according to the magnification, and emits collimated light. In terms of imaging, the object is placed at infinity (defined as the distance at which light rays can be considered collimated) in relation to the optical elements and relayed an infinite distance. No image is formed, but can be with the introduction of a secondary infinite/ finite conjugate design system.

Infrared (IR) Spectrum

The wavelength interval of the electromagnetic spectrum that corresponds to infrared light (light that is beyond the visible red range). IR radiation is often divided into three smaller regions: 0.750 - 3μm, 3 - 30μm, and 30 - 1000μm – defined as near-infrared (NIR), mid-wave infrared (MWIR), and far-infrared (FIR), respectively.

Integration Time

In an imaging device, the length of time during which the sensing elements are collecting charge between transfers to the transport registers. Also known as exposure time.

Interference Filter

A type of filter made up of several metallic or dielectric layers of material, typically composing a three-cavity design. The correct combination yields high spectral transmittance over very narrow wavelength ranges due to interference effects between layers.

  See also Filter , Dielectric Coating

Interference Fringe

Alternating light and dark bands in an intensity pattern due to the wave nature of light.  The phase difference remains constant along one fringe.  When using an optical flat, straight, parallel, and evenly spaced interference fringes indicate that the work surface flatness is equal to or higher than that of the reference surface.

Interferometry

A family of techniques that utilizes the interference of waves of light for precise determinations of, wavelength, flatness, or other attributes.

Interlaced Scan

Interlaced imaging devices produce images by scanning and reading out odd-numbered lines in the first pass, then even-numbered lines in the second pass, and so on. Two fields are assembled into one full frame. 

  See also Field , Progressive Scan

Interline Transfer

Also referred to as 2:1 interlaced video, it combines two fields to make up each video. If each field is scanned at 60Hz, the frame rate is necessarily 30Hz.

  See also Frame

Inverted Load Capacity

The reverse, or inverse, or normal load capacity whereby the load or force applied to a mechanical component is directed upward. 

  See also Normal Load Capacity

Ion-Beam Sputtering (IBS)

A physical vapor depostition technique to increase the density of thin-film coatings, thus creating "hard coated" filters. The thin film is deposited by sputtering (ejecting) material from a target by ion bombardment which is then deposited onto the filter substrate.

Iris Diaphragm

A mechanical aperture designed to smoothly change the aperture size. It can be used to control the amount of light entering an optical system if used as the aperture stop. 

  See also Aperture (f/#) , Aperture Stop

Irradiance

Denoted by E, it is the incident power per unit area, measured in W/m2. Also known as radiant flux density.

Irregularity

A type of surface accuracy specification that describes how the shape of a surface deviates from the shape of a reference surface. Regularity refers to the sphericity of the circular fringes that are formed from the comparison of the test surface to the reference surface.  When the power of a surface is more than 5 fringes, it is difficult to detect small irregularities of less than 1 fringe. So surfaces are specified with a ratio of power to irregularity of approximately 5:1. 

Spherical optics, aspheric lenses, prisms, imaging lenses, imaging and laser optics assemblies, and mechanics are just a few of our expertise.

Edmund Optics' engineers are experts in delivering the best solution possible. From stock products to custom designs, EO has the industry and technical knowledge to help meet your needs.

Over 15 regional offices in the Americas, Europe, and Asia to offer local support with world-class service.

Need to contact Edmund Optics? Use any of our fast and friendly services to meet your needs.

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram

×