Edmund Optics uses cookies to optimise and enhance the features and content on our website. By continuing to use this website, you consent to our use of cookies.

  • My Account
  •   
Resources / Application Notes / Optics / How to Select the Right Light Pipe Homogenizing Rod
How to Select the Right Light Pipe Homogenizing Rod
Edmund Optics Inc.

How to Select the Right Light Pipe Homogenizing Rod

Light Pipe Homogenizing Rods

Much like optical fibers, light pipe homogenizing rods utilize total internal reflection (TIR) to transmit light from the entrance to the exit of the light pipe. The substrate’s refractive index is the only factor that influences the light pipe’s critical angle, which defines the angle of acceptance at which TIR will occur. Light pipes designed specifically for high NA, standard NA, and low NA light sources will have the same acceptance angle if designed with the same substrate.

The critical angle (θc) calculated using Equation 1:

Equation 1 (1)

In the case of an N-BK7 light pipe, the index of refraction at Helium’s d-line of 587.9nm is 1.517, resulting in a θc of 41°. If the incident angle is greater than θc, TIR will occur and light will be transmitted throughout the light pipe (Figure 1).

Since light rays enter a light pipe at a variety of incident angles, the number of reflections inside the light pipe differs from ray to ray. The smallest incident angle, which is equal to θc, will have more reflections than light entering at an incident angle that is many times larger than θc within the same length light pipe (Figure 2).

Due to low NA light sources having a larger number of rays greater than θc than high NA light sources, low NA light pipes are longer than high NA light pipes, and are recommended for light sources with narrow beam divergence.

Note: Light pipes are not designed for use with collimated laser sources. To homogenize collimated light sources, Microlens Arrays or flat top laser beam shapers are recommended. Light pipes are ideal for homogenizing polychromatic sources that emit non-collimated light.

Total Internal Reflection in a Light Pipe Homogenizing Rod
Figure 1: Total Internal Reflection (TIR) in a Light Pipe Homogenizing Rod
Small Incident Angles Have More Reflections than Large Incident Angles
Figure 2: Small Incident Angles Have More Reflections than Large Incident Angles

Was this content useful to you?

Understand the optical theories behind prism geometries to select the best prism for any application.

Whether you need a prism for image displacement, laser beam steering, or dispersion, we have an optical component for you or we can make it for you. 

Homogenize non-uniform UV or visible light sources. Hexagonal or tapered configurations available.

What is interference? How does Snell’s Law work? Read this easy- to-follow, introductory content for anyone interested in learning the foundations of optical theory.

Prisms are useful for folding optical systems or rotating images. Learn about the important concepts to remember when choosing a prism.

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Google+ Edmund Optics Instagram

×